Headquarters

  • Universal Robots A/S
  • Energivej 25
  • DK-5260 Odense S
  • Denmark 
  • Find your regional contact here
 

World wide

  • Americas headquarter
  • Universal Robots USA, Inc.
  • 5430 Data Court, Suite 300
    Ann Arbor, Michigan 48108, USA
  • Tel. +1 844 462-6268
  • ur.na@universal-robots.com

  • Southern Europe, MEA, Turkey
  • Universal Robots Spain S.L
  • c/Josep Plà 2 –  Edificio B2
  • Planta baja, local C
  • E-08019 Barcelona, SPAIN
  • Tel. +34 933 158 076
  • ur.med@universal-robots.com
  • Central and Eastern Europe
  • Universal Robots A/S
  • Siemensova 2717/4
  • 150 00 Praha 13 – Stodůlky
  • Czech Republic
  • Tel. +420 222 286 200
  • ur.cee@universal-robots.com

 

 
  • APAC
  • Universal Robots (Singapore) Pte, Ltd.
  • 20 Science Park Road, Teletech Park
    Science Park II, #03-36/37,
    SINGAPORE 117674
  • Tel. +65 66 35 72 70
  • ur.apac@universal-robots.com

  • India
  • Universal Robots India Pvt. Ltd
  • Ground floor, Beech, E1 Manyata Embassy Business Park
    Outer Ring Road, Nagawara
    Bangalore 560045
  • Tel. +91 97428 22033
  • ur.india@universal-robots.com
 
  • China
  • Universal Robots (Shanghai) Ltd.
  • Room 2008, 20th Floor 
    No. 688 West Nanjing Road 
    Jingan District
  • 200041 PRC, Shanghai, CHINA
  • Tel. +86 21 6132 6418
  • ur.china@universal-robots.com
For Technical Support, please contact your Local distributor
Find distributor

Click here

05. October 2017
Blog>Cobots in Lights-Out Manufacturing? Collaboration Works Even When Humans Aren’t.

Cobots in Lights-Out Manufacturing? Collaboration Works Even When Humans Aren’t.

The idea of using collaborative robots for lights-out manufacturing can seem like a contradiction in terms. After all, cobots differ from traditional robots by being able to work side-by-side with human workers, and lights-out manufacturing is a human-free automation approach. But the collaborative aspect of cobots is more than just the ability to share a work cell. Cobots are also defined by their affordability, flexibility, and ease-of-use—traits that are critical for new lights-out applications.

Lights-out manufacturing is getting smaller

Factories with no humans in sight are still rare, and are typically limited to extremely high-volume, high-cost operations. The vast majority of manufacturers are small and mid-sized enterprises (SMEs), with limited automation budgets to support what is often low-volume, high-mix, or changeable applications.

Many SMEs are interested in a lights-out approach for third-shift operations or to address seasonal peaks. In today’s market, where manufacturers are struggling to hire and retain workers as well as meet quality and delivery expectations, those additional shifts can be difficult—and expensive—to staff. In other situations, manufacturers may choose to use lights-out automation for specific processes that are unsuitable or unsafe for human workers to be around, such as those that involve extreme temperatures or noxious gases.

A-UR5-robot-now-allows-Whippany-Actuation-Systems-to-run-two-shifts-unattended.jpg
A UR5 robot now allows Whippany Actuation Systems to run two shifts unattended

Invest in additional CNC machine, or increase capacity of the one in-house?

New Jersey-based Whippany Actuation Systems makes components for the aerospace and defense industries. When the company suddenly needed to increase capacity, the options were to make a significant investment in an additional CNC machine or to make better use of the one in-house. A UR cobot with adaptive gripper now handles multiple part sizes and allows Whippany to run two additional unattended shifts using the existing CNC machine.

Phil De Mauro, Whippany manufacturing engineering leader, said, “We’ve added capacity by being able to run the machine during unattended hours, but it’s also freed-up skilled workers to do other tasks as opposed to loading and unloading the machine—it frees them up to do more valued-added activities.”

Lights-out automation has helped Whippany meet its increased productivity goals, but it also helps in other factors, such as improved margins, increased competitiveness, and shortened lead time. Read the full Whippany case study.

UR3-robot-can-be-directly-monitored-on-his-phone.jpg
CEO of Creating Revolutions, Einar Rosenberg, receives performance data of the UR3 robot directly on his phone that receives production data and alerts in real-time

Cobot stays up late to be ready for human workers in the morning

Creating Revolutions is a Florida-based startup that makes a customer-service paging system for the hospitality industry. As a startup, budgets are tight, but the company was struggling to meet demand and maintain quality in its product’s complex assembly process. The solution was an affordable, easy-to-program UR cobot integrated by Hirebotics in an innovative rental model in which Creating Revolutions pays only for the hours the cobot operates.

Creating-Revolutions-can-monitor-the-robot-remotely.jpg

The cobot solves the manufacturer’s need for accuracy and through-put while working alongside human workers during the day. But the cobot also continues to perform long after workers go home for the night, preparing parts for assembly the next day.





Creating Revolutions can monitor the robot remotely trough a web cam that streams directly to mobile devices


Hirebotics Co-founder Matt Bush says, “Most companies are years away from lights-out manufacturing because it’s so capital intensive. But by renting robots by the hour, and only paying for the hours they actually work, companies of all sizes can afford to automate more of their processes.” Hirebotics’ cloud-connected solution includes high-definition cameras and a web-based interface that lets the manufacturer and Hirebotics monitor the robot on any smartphone. The software also provides insight into precise production data around the clock.
Read the full Creating Revolutions case study.


UR10-robot-runs-overnight-at-Voodoo-Manufacturing.jpg
By running the UR10 robot overnight, Voodoo Manufacturing is able to triple production output

Round-the-clock production helps startup scale up

Voodoo Manufacturing in Brooklyn, New York is a rapidly growing 3D printing farm that is scaling up to handle large production runs to compete with traditional plastic injection molding manufacturing. “Harvesting” is the process of loading and unloading 3D printer plates, which takes up about 10% of all labor hours. This repetitive task requires speed, accuracy, and consistency—making it ideal for automation. And using UR cobots allows the company to automate at about one-fifth the cost of traditional robotics that require safety cages and expensive integration.

Voodoo installed the cobot on a mobile base so it can tend up to one hundred 3D printers. With a second cobot, the startup will go from 30%-40% printer utilization to 90%. The key to tripling output is the ability for the cobot to tend printers overnight.

Jonathan Schwartz, Chief Product Officer of Voodoo Manufacturing, says, “We can monitor the robot through our own software and access the status of any given printer to see whether it’s printing or idle, which means we can deploy this in our factory and run it 24/7 without any human oversight.” Schwartz describes the first morning he came in to find more than 30 completed print runs handled overnight as “magical.” Read the full Voodoo Manufacturing case study.

Voodoo-Manufacturing,-programs-the-UR10-robot.jpg
Jonathan Schwartz, Chief Product Officer at Voodoo Manufacturing, programs the UR10 robot

Cobots Make Lights-Out Manufacturing a Reality—Even for Small Operations

Affordable, flexible, and easy-to-use cobots are making lights-out manufacturing an option even for smaller operations. With the addition of innovative Industry 4.0 technologies, companies can monitor what’s happening after the lights go out, and enjoy the increased output when workers arrive in the morning.

Get your team on-board with cobots book cover.png

 

 

 

 



Download the ebook “Get Your Team On Board with Cobots” 

Share this post

Universal Robots

We believe that collaborative robotic technology can be used to benefit all aspects of task-based businesses – no matter what their size.

We believe that the latest collaborative robot technology should be available to all businesses. The nominal investment cost is quickly recovered as our robotic arms have an average payback period of just six months.

Comments

About UR Blog

Find inspiring stories on how collaborative robots - or cobots - are lowering the automation barrier. And learn how the UR cobots can benefit your business.

Enjoy.

Categories

    Recent posts

    ¨